Skip to main content
Visitor II
August 26, 2025
Solved

LTDC Controller not displaying image

  • August 26, 2025
  • 2 replies
  • 518 views

I am currently using the STM32N657 on the NUCLEO-N657X0-Q board to drive an 800x480 pixel display with 24-bit color. The display that I am using is the NHD-7.0-800480EF-ASXV#-T. I’m using the built in LTDC controller on the chip. I do know that the controller is working because the entire screen is black, the screen would be showing the backlight if it wasn’t. The problem is that I am unable to display anything at all when writing to the screen buffer.

Here are the configuration parameters that I am using based on the data sheet:

DHOUT19_0-1756245275614.png

Here are the layer settings that I am using:

DHOUT19_1-1756245305699.png

Here is the clock configuration for the LTDC:

DHOUT19_2-1756245348090.png

 

Here is the code that I am running:

main.c

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ICACHE_Init();
 MX_LTDC_Init();
 MX_RAMCFG_Init();
 /* USER CODE BEGIN 2 */
 hal_pointers_t halPointers = {0};
 halPointers.hltdc = &hltdc;
 /* USER CODE END 2 */

 /* Initialize leds */
 BSP_LED_Init(LED_BLUE);
 BSP_LED_Init(LED_RED);
 BSP_LED_Init(LED_GREEN);

 /* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/
 BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);

 /* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */
 BspCOMInit.BaudRate = 115200;
 BspCOMInit.WordLength = COM_WORDLENGTH_8B;
 BspCOMInit.StopBits = COM_STOPBITS_1;
 BspCOMInit.Parity = COM_PARITY_NONE;
 BspCOMInit.HwFlowCtl = COM_HWCONTROL_NONE;
 if (BSP_COM_Init(COM1, &BspCOMInit) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 __HAL_RCC_AXISRAM3_MEM_CLK_ENABLE();
 __HAL_RCC_AXISRAM4_MEM_CLK_ENABLE();
 __HAL_RCC_AXISRAM5_MEM_CLK_ENABLE();
 __HAL_RCC_AXISRAM6_MEM_CLK_ENABLE();

 HAL_RAMCFG_EnableAXISRAM(&hramcfg_SRAM3);
 HAL_RAMCFG_EnableAXISRAM(&hramcfg_SRAM4);
 HAL_RAMCFG_EnableAXISRAM(&hramcfg_SRAM5);
 HAL_RAMCFG_EnableAXISRAM(&hramcfg_SRAM6);

 main_app(halPointers);
 while (1)
 {

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

main_app function

#include "main_application.h"

__attribute__((section(".screen_buffer")))
uint8_t screen_buffer[FRAME_BUFFER_SIZE];

void main_app(hal_pointers_t hal_pointers){

	for (uint32_t i = 0; i < FRAME_BUFFER_SIZE; i++){
		screen_buffer[i] = 0;
	}


	HAL_LTDC_SetAddress(hal_pointers.hltdc, (uint32_t) screen_buffer, 0);
	//HAL_LTDC_ReloadLayer(hal_pointers.hltdc, LTDC_RELOAD_IMMEDIATE, 0);
	//HAL_LTDC_SetOutputDisplay(hal_pointers.hltdc, LTDC_OUT_RGB);

	//Make a square
	for (uint32_t i = 0; i < FRAME_BUFFER_SIZE/3; i++){
		//for (uint32_t j = 0; j < 20; j++){
			//screen_buffer[(i*3) + (j*SCREEN_WIDTH*3)] = 255;
			screen_buffer[i*3] = 0x55;
		//}
	}

	while(1){
	}

}

Linker Script (Just in case):

/*
******************************************************************************
**
** @file : STM32N6XX_AXISRAM2_fsbl.ld
**
** @author : GPM Application Team
**
** @brief : Linker script for STM32N6XX Device from STM32N6 series
** 512 KBytes RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used
**
** Target : STMicroelectronics STM32
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
******************************************************************************
** @attention
**
** Copyright (c) 2025 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
******************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
_sstack = _estack - _Min_Stack_Size;

_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x800; /* required amount of stack */

/* Memories definition */
MEMORY
{
 ROM (xrw) : ORIGIN = 0x34180400, LENGTH = 255K
 RAM (xrw) : ORIGIN = 0x341C0000, LENGTH = 256K
 SCREEN_BUFFER_SRAM (rw) : ORIGIN = 0x34200000, LENGTH = 1300K
}

/* Sections */
SECTIONS
{
 /* The startup code into "RAM" Ram type memory */
 .isr_vector :
 {
 . = ALIGN(4);
 KEEP(*(.isr_vector)) /* Startup code */
 . = ALIGN(4);
 } >ROM

 /* The program code and other data into "RAM" Ram type memory */
 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)
 *(.RamFunc) /* .RamFunc sections */
 *(.RamFunc*) /* .RamFunc* sections */

 KEEP (*(.init))
 KEEP (*(.fini))

 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >ROM

 /* Constant data into "RAM" Ram type memory */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >ROM

 .ARM.extab (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 *(.ARM.extab* .gnu.linkonce.armextab.*)
 . = ALIGN(4);
 } >ROM

 .ARM (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 . = ALIGN(4);
 } >ROM

 .preinit_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 . = ALIGN(4);
 } >ROM

 .init_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 . = ALIGN(4);
 } >ROM

 .fini_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 . = ALIGN(4);
 } >ROM

 /* Used by the startup to initialize data */
 _sidata = LOADADDR(.data);

 /* Initialized data sections into "RAM" Ram type memory */
 .data :
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */

 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */

 } >RAM AT> ROM

 .noncacheable :
 {
 . = ALIGN(8);
 __snoncacheable = .;/* create symbol for start of section */
 KEEP(*(.noncacheable))
 . = ALIGN(8);
 __enoncacheable = .; /* create symbol for end of section */
 } > RAM


 .gnu.sgstubs :
 {
 . = ALIGN(4);
 *(.gnu.sgstubs*) /* Secure Gateway stubs */
 . = ALIGN(4);
 } >ROM
 /* Uninitialized data section into "RAM" Ram type memory */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss section */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)

 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM

 /* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
 ._user_heap_stack :
 {
 . = ALIGN(8);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
 } >RAM

 /* Remove information from the compiler libraries */
 /DISCARD/ :
 {
 libc.a ( * )
 libm.a ( * )
 libgcc.a ( * )
 }
 
 .screen_buffer (NOLOAD) :
 {
 	. = ALIGN(4);
 	_screen_buffer_start = .;
 	KEEP(*(.screen_buffer))
 	. = ALIGN(4);
 	_screen_buffer_end = .;
 } > SCREEN_BUFFER_SRAM

 .ARM.attributes 0 : { *(.ARM.attributes) }
}

Here is what I’ve observed:

- I have run the code in debug mode and can see data being written at the screen buffer location

- I’ve hooked up a logic analyzer to the red data pins, HSYNC, VSYNC, DE, and DCLK (below is a snapshot). When the red data pins are not active HSYNC seems to be acting somewhat normally. When the data pins are active, HSYNC does not act normal at all. It pulses almost randomly. Please note that the logic analyzer is a cheap one from Amazon, so it may not even be reading this data correctly.

DHOUT19_3-1756245465102.png

DHOUT19_4-1756245505638.png

 

Here's what I’ve tried:

- I’ve tried using the following HAL functions: HAL_LTDC_ReloadLayer(hal_pointers.hltdc, LTDC_RELOAD_IMMEDIATE, 0), HAL_LTDC_SetOutputDisplay(hal_pointers.hltdc, LTDC_OUT_RGB). No change

- I’ve tried slightly adjusting the pulse width settings for both HSYNC and VSYNC. No change.

 

Let me know if I’ve forgotten to provide any information.

    This topic has been closed for replies.
    Best answer by DHOUT19

    To anyone who stumbles upon this post. I figured out what my issue was. I was using AXISRAM to store my screen's buffer memory, which by itself is fine. What I didn't realize is that the LTDC peripheral does not initially have access to this memory. In order for the display data to get to the LTDC peripheral, you need to use the RIMU.

    DHOUT19_0-1756382424563.png

    In order to enable the RIMU you need to enable RIF in the hardware configuration. Make sure to enable it whether you are running your main code in application or in FSBL.

    DHOUT19_1-1756382864708.png

    Then go to the RIF tab on the top, go to "Domains (RIMU)" tab on the side, and then give LTDC_L1 (Layer 1, or whichever Layer(s) you are using) privilege and secure status. The way that I understand it, you are telling the microcontroller that the LTDC can have full access to system resources (privilege) and is a trusted peripheral (secure).

    DHOUT19_2-1756382989874.png

    Once you do that, you need to add these lines of code.

     RIMC_MasterConfig_t RIMC_master = {0};
     RIMC_master.MasterCID = RIF_CID_1;
     RIMC_master.SecPriv = RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV;
     HAL_RIF_RIMC_ConfigMasterAttributes(RIF_MASTER_INDEX_LTDC1 , &RIMC_master);
    
     HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_LTDCL1 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV);


    These lines of code basically do what the hardware configurator is supposed to do. I'm not really sure why the hardware configurator doesn't write these lines of code for you, unless it's not being written in main.c. You will want to write these lines of code before you set the memory address or addresses for any of your LTDC layers.

    As soon as I added these lines of code, I immediately saw color on my screen.
    20250827_171430.jpg

    2 replies

    ST Employee
    August 28, 2025

    Hello @DHOUT19  ,

    Could you please provide details on how you have connected the NHD-7.0-800480EF-ASXV#-T display to the NUCLEO-N657X0-Q board?

     

    br

    DHOUT19AuthorAnswer
    Visitor II
    August 28, 2025

    To anyone who stumbles upon this post. I figured out what my issue was. I was using AXISRAM to store my screen's buffer memory, which by itself is fine. What I didn't realize is that the LTDC peripheral does not initially have access to this memory. In order for the display data to get to the LTDC peripheral, you need to use the RIMU.

    DHOUT19_0-1756382424563.png

    In order to enable the RIMU you need to enable RIF in the hardware configuration. Make sure to enable it whether you are running your main code in application or in FSBL.

    DHOUT19_1-1756382864708.png

    Then go to the RIF tab on the top, go to "Domains (RIMU)" tab on the side, and then give LTDC_L1 (Layer 1, or whichever Layer(s) you are using) privilege and secure status. The way that I understand it, you are telling the microcontroller that the LTDC can have full access to system resources (privilege) and is a trusted peripheral (secure).

    DHOUT19_2-1756382989874.png

    Once you do that, you need to add these lines of code.

     RIMC_MasterConfig_t RIMC_master = {0};
     RIMC_master.MasterCID = RIF_CID_1;
     RIMC_master.SecPriv = RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV;
     HAL_RIF_RIMC_ConfigMasterAttributes(RIF_MASTER_INDEX_LTDC1 , &RIMC_master);
    
     HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_LTDCL1 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV);


    These lines of code basically do what the hardware configurator is supposed to do. I'm not really sure why the hardware configurator doesn't write these lines of code for you, unless it's not being written in main.c. You will want to write these lines of code before you set the memory address or addresses for any of your LTDC layers.

    As soon as I added these lines of code, I immediately saw color on my screen.
    20250827_171430.jpg

    Explorer
    December 27, 2025

    A good 16 hours lost between reading manuals, debug attempts, and ChatGPT ended up with a big fat nothing. This post fixed it in seconds. This *really* should be added to AN4861. Thank you for coming back and making such a great post!