Skip to main content
Graduate II
October 24, 2024
Question

LTDC Display Type Restriction

  • October 24, 2024
  • 2 replies
  • 703 views

I am using the STM32H743VIT and trying to integrate using LTDC. The Display Type options in CUBEMX only allow 16 or 18 bit RGB. I know there is no LTDC_R0, so I assume that is why there is not option for 24 bit RGB; however, we were just planning on tying the LSB R value low to work around this issue. Is there any information on how to set this MCU up for 24bit RBG even though CUBEMX does not allow it?

 

Thank you

EDIT: I am using the 100 pin LQFP package

    This topic has been closed for replies.

    2 replies

    ST Employee
    October 25, 2024

    Hello @EthanMankins ,

    Thank you for reaching out with your issue regarding the STM32H743VIT and LTDC integration in CubeMX.

    I have tried a project with the same board and found that the option for 24-bit RGB (RGB888) is indeed available. Please see the screenshot below for reference:

     

    MOBEJ_1-1729866104175.png

     

    In the LTDC Mode and Configuration section under the "Multimedia" category, you should be able to select "RGB888 (24 bits)" from the Display Type dropdown menu.

    If you still do not see the 24-bit option, please ensure that you are using the latest version of CubeMX. Updating CubeMX might resolve any discrepancies.

    Br

     

    Graduate II
    October 25, 2024

    @MOBEJ 
    Sorry I didn't clarify I'm using the 100 pin LQFP Version.

    I just updated and still do not see the 24 option

    Graduate
    April 15, 2025

    Hello1.png, can you tell me if you have been able to solve this problem?
    I am facing the same problem with STM32h743vit6

    CubeMX ver. 6.14.1

     

    Did I understand correctly that LQFP-100 does not support RGB888 at all, unlike LQFP-176 ( STM32H743IIT6 )
    What is the reason for this? There are enough physical pins for RGB888.