MIPI-DSI LTDC configuration lcd
Hello everyone, I need help with a DSI + LTDC configuration.
I'm working on a custom board with an STM32H747BIT and trying to drive a 720x1280 RGB888 display without GRAM, using the ILI9881C controller via DSIHOST + LTDC.
Here’s the situation:
I’m currently testing at 500 Mbps per DSI lane (i.e., 62.5 MHz per lane, 2 lanes total) and 50 MHz LTDC pixel clock.
The built-in test pattern works fine, but when I try to draw using the framebuffer, the image is misaligned, sometimes flickers, and the drawing coordinates are not correct.
For example, when I try to draw two horizontal bands, the first one appears larger than expected.
I suspect it’s related to timing parameters like HSA, HBP, HFP, VSA, VBP, VFP – but the datasheet for the display doesn't provide them.
Observations and questions:
To get the correct colors, I had to set ARGB8888 in LTDC, even though the display is RGB888.
Without the missing timing values, I can’t estimate the frame rate or configure DSI properly — I’m stuck.
Is there a reliable method to empirically find working H/V timing values?
The display I'm using is: RF3500D-AYW-MNG1-000
Is there anything that needs to be configured in the ILI9881C controller to make this work properly?
In the main code, I simply write to the framebuffer at 0xC0000000, then call HAL_DSI_Start(). No other logic is running yet.
Any help or working example would be greatly appreciated :folded_hands:
static void MX_DSIHOST_DSI_Init(void)
{
/* USER CODE BEGIN DSIHOST_Init 0 */
/* USER CODE END DSIHOST_Init 0 */
DSI_PLLInitTypeDef PLLInit = {0};
DSI_HOST_TimeoutTypeDef HostTimeouts = {0};
DSI_PHY_TimerTypeDef PhyTimings = {0};
DSI_VidCfgTypeDef VidCfg = {0};
/* USER CODE BEGIN DSIHOST_Init 1 */
/* USER CODE END DSIHOST_Init 1 */
hdsi.Instance = DSI;
hdsi.Init.AutomaticClockLaneControl = DSI_AUTO_CLK_LANE_CTRL_DISABLE;
hdsi.Init.TXEscapeCkdiv = 4;
hdsi.Init.NumberOfLanes = DSI_TWO_DATA_LANES;
PLLInit.PLLNDIV = 20;
PLLInit.PLLIDF = DSI_PLL_IN_DIV1;
PLLInit.PLLODF = DSI_PLL_OUT_DIV1;
if (HAL_DSI_Init(&hdsi, &PLLInit) != HAL_OK)
{
Error_Handler();
}
HostTimeouts.TimeoutCkdiv = 1;
HostTimeouts.HighSpeedTransmissionTimeout = 0;
HostTimeouts.LowPowerReceptionTimeout = 0;
HostTimeouts.HighSpeedReadTimeout = 0;
HostTimeouts.LowPowerReadTimeout = 0;
HostTimeouts.HighSpeedWriteTimeout = 0;
HostTimeouts.HighSpeedWritePrespMode = DSI_HS_PM_DISABLE;
HostTimeouts.LowPowerWriteTimeout = 0;
HostTimeouts.BTATimeout = 0;
if (HAL_DSI_ConfigHostTimeouts(&hdsi, &HostTimeouts) != HAL_OK)
{
Error_Handler();
}
PhyTimings.ClockLaneHS2LPTime = 20;
PhyTimings.ClockLaneLP2HSTime = 18;
PhyTimings.DataLaneHS2LPTime = 10;
PhyTimings.DataLaneLP2HSTime = 13;
PhyTimings.DataLaneMaxReadTime = 0;
PhyTimings.StopWaitTime = 0;
if (HAL_DSI_ConfigPhyTimer(&hdsi, &PhyTimings) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_ConfigFlowControl(&hdsi, DSI_FLOW_CONTROL_BTA) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_SetLowPowerRXFilter(&hdsi, 10000) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_ConfigErrorMonitor(&hdsi, HAL_DSI_ERROR_NONE) != HAL_OK)
{
Error_Handler();
}
VidCfg.VirtualChannelID = 0;
VidCfg.ColorCoding = DSI_RGB888;
VidCfg.LooselyPacked = DSI_LOOSELY_PACKED_DISABLE;
VidCfg.Mode = DSI_VID_MODE_BURST;
VidCfg.PacketSize = 720;
VidCfg.NumberOfChunks = 1;
VidCfg.NullPacketSize = 0;
VidCfg.HSPolarity = DSI_HSYNC_ACTIVE_LOW;
VidCfg.VSPolarity = DSI_VSYNC_ACTIVE_LOW;
VidCfg.DEPolarity = DSI_DATA_ENABLE_ACTIVE_HIGH;
VidCfg.HorizontalSyncActive = (ILI9881C_720X1280_HSYNC * 62500U)/27429U;
VidCfg.HorizontalBackPorch = (ILI9881C_720X1280_HBP * 62500U)/27429U;
VidCfg.HorizontalLine = ((720 + ILI9881C_720X1280_HSYNC + ILI9881C_720X1280_HBP + ILI9881C_720X1280_HFP) * 62500U)/27429U;
VidCfg.VerticalSyncActive = ILI9881C_720X1280_VSYNC;
VidCfg.VerticalBackPorch = ILI9881C_720X1280_VBP;
VidCfg.VerticalFrontPorch = ILI9881C_720X1280_VFP;
VidCfg.VerticalActive = 1280;
VidCfg.LPCommandEnable = DSI_LP_COMMAND_DISABLE;
VidCfg.LPLargestPacketSize = 0;
VidCfg.LPVACTLargestPacketSize = 0;
VidCfg.LPHorizontalFrontPorchEnable = DSI_LP_HFP_ENABLE;
VidCfg.LPHorizontalBackPorchEnable = DSI_LP_HBP_ENABLE;
VidCfg.LPVerticalActiveEnable = DSI_LP_VACT_ENABLE;
VidCfg.LPVerticalFrontPorchEnable = DSI_LP_VFP_ENABLE;
VidCfg.LPVerticalBackPorchEnable = DSI_LP_VBP_ENABLE;
VidCfg.LPVerticalSyncActiveEnable = DSI_LP_VSYNC_ENABLE;
VidCfg.FrameBTAAcknowledgeEnable = DSI_FBTAA_DISABLE;
if (HAL_DSI_ConfigVideoMode(&hdsi, &VidCfg) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_SetGenericVCID(&hdsi, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DSIHOST_Init 2 */
RCC_PeriphCLKInitTypeDef PeriphClkInit;
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_DSI;
PeriphClkInit.DsiClockSelection = RCC_DSICLKSOURCE_PHY;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit);
/* USER CODE END DSIHOST_Init 2 */
}
static void MX_LTDC_Init(void)
{
/* USER CODE BEGIN LTDC_Init 0 */
__HAL_RCC_LTDC_CLK_ENABLE();
/* USER CODE END LTDC_Init 0 */
LTDC_LayerCfgTypeDef pLayerCfg = {0};
/* USER CODE BEGIN LTDC_Init 1 */
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/* Configura PLL3 per fornire clock a LTDC */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC;
PeriphClkInitStruct.PLL3.PLL3M = 1; //5; //27.5Mhz
PeriphClkInitStruct.PLL3.PLL3N = 6; //132;
PeriphClkInitStruct.PLL3.PLL3R = 3; //3;
PeriphClkInitStruct.PLL3.PLL3P = 2; //2;
PeriphClkInitStruct.PLL3.PLL3Q = 2; //24;
PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_1;
PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL3VCOMEDIUM;
PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* USER CODE END LTDC_Init 1 */
hltdc.Instance = LTDC;
hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AH;
hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
hltdc.Init.HorizontalSync = ILI9881C_720X1280_HSYNC - 1;
hltdc.Init.VerticalSync = ILI9881C_720X1280_VSYNC - 1;
hltdc.Init.AccumulatedHBP = ILI9881C_720X1280_HSYNC + ILI9881C_720X1280_HBP - 1;
hltdc.Init.AccumulatedVBP = ILI9881C_720X1280_VSYNC + ILI9881C_720X1280_VBP - 1;
hltdc.Init.AccumulatedActiveW = ILI9881C_720X1280_HSYNC + 720 + ILI9881C_720X1280_HBP - 1;
hltdc.Init.AccumulatedActiveH = ILI9881C_720X1280_VSYNC + 1280 + ILI9881C_720X1280_VBP - 1;
hltdc.Init.TotalWidth = ILI9881C_720X1280_HSYNC + 720 + ILI9881C_720X1280_HBP + ILI9881C_720X1280_HFP - 1;
hltdc.Init.TotalHeigh = ILI9881C_720X1280_VSYNC + 1280 + ILI9881C_720X1280_VBP + ILI9881C_720X1280_VFP - 1;
hltdc.Init.Backcolor.Blue = 0;
hltdc.Init.Backcolor.Green = 0;
hltdc.Init.Backcolor.Red = 0;
if (HAL_LTDC_Init(&hltdc) != HAL_OK)
{
Error_Handler();
}
pLayerCfg.WindowX0 = 0;
pLayerCfg.WindowX1 = 720;
pLayerCfg.WindowY0 = 0;
pLayerCfg.WindowY1 = 1280;
pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_ARGB8888;
pLayerCfg.Alpha = 255;
pLayerCfg.Alpha0 = 0;
pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
pLayerCfg.FBStartAdress = 0xC0000000;
pLayerCfg.ImageWidth = 720;
pLayerCfg.ImageHeight = 1280;
pLayerCfg.Backcolor.Blue = 0;
pLayerCfg.Backcolor.Green = 0;
pLayerCfg.Backcolor.Red = 0;
if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN LTDC_Init 2 */
/* USER CODE END LTDC_Init 2 */
}