Skip to main content
Visitor II
July 5, 2024
Solved

Need Help to generate changing frequency sine wave in STM32L073RZT

  • July 5, 2024
  • 2 replies
  • 2471 views

Hello Community,

I'm working on a project and could use your help. I'm trying to make a sine wave with a changing frequency from 600 Hz to 5 kHz using STM32 microcontroller(STM32L073RZT) with 32 MHz as sysclk.Capture.PNG

 

Capture1.PNG

Capture2.PNG

This are my configurations. Where this r2r pins are DAC bits. 

 

I am not able to generate sine wave more than 280 Hz but i want to generate till 2 KHz. 

Please suggest if I'm doing something wrong or if anyone has a good idea on how to overcome this issue.

 

Code: 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include <stdio.h>
#include "stm32l0xx.h"
#include <math.h>
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define SINE_TABLE_SIZE 256
void output_to_dac(uint16_t value);
volatile uint32_t Index = 0;
volatile uint32_t stepSize = 1;
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim2;

UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM2_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
const uint16_t sineLookupTable[] = {
128, 131, 134, 137, 140, 143, 146, 149, 152, 155,
158, 162, 165, 167, 170, 173, 176, 179, 182, 185,
188, 190, 193, 196, 198, 201, 203, 206, 208, 211,
213, 215, 218, 220, 222, 224, 226, 228, 230, 232,
234, 235, 237, 238, 240, 241, 243, 244, 245, 246,
248, 249, 250, 250, 251, 252, 253, 253, 254, 254,
254, 255, 255, 255, 255, 255, 255, 255, 254, 254,
254, 253, 253, 252, 251, 250, 250, 249, 248, 246,
245, 244, 243, 241, 240, 238, 237, 235, 234, 232,
230, 228, 226, 224, 222, 220, 218, 215, 213, 211,
208, 206, 203, 201, 198, 196, 193, 190, 188, 185,
182, 179, 176, 173, 170, 167, 165, 162, 158, 155,
152, 149, 146, 143, 140, 137, 134, 131, 128, 124,
121, 118, 115, 112, 109, 106, 103, 100, 97, 93,
90, 88, 85, 82, 79, 76, 73, 70, 67, 65,
62, 59, 57, 54, 52, 49, 47, 44, 42, 40,
37, 35, 33, 31, 29, 27, 25, 23, 21, 20,
18, 17, 15, 14, 12, 11, 10, 9, 7, 6,
5, 5, 4, 3, 2, 2, 1, 1, 1, 0,
0, 0, 0, 0, 0, 0, 1, 1, 1, 2,
2, 3, 4, 5, 5, 6, 7, 9, 10, 11,
12, 14, 15, 17, 18, 20, 21, 23, 25, 27,
29, 31, 33, 35, 37, 40, 42, 44, 47, 49,
52, 54, 57, 59, 62, 65, 67, 70, 73, 76,
79, 82, 85, 88, 90, 93, 97, 100, 103, 106,
109, 112, 115, 118, 121, 124};


void setFrequency(uint32_t frequency) {
 printf("1Timer Period for %u Hz\n", frequency);
 uint32_t timer_period = (32000000 / (SINE_TABLE_SIZE * frequency)) - 1;
 printf("Timer Period for %u Hz: %u\n", frequency, timer_period);
 __HAL_TIM_SET_AUTORELOAD(&htim2, timer_period);
 
}

void output_to_dac(uint16_t value){
 HAL_GPIO_WritePin(GPIOB,r2r_0_Pin,(value & 0x01) ? GPIO_PIN_SET : GPIO_PIN_RESET);
 HAL_GPIO_WritePin(GPIOB,r2r_1_Pin,(value & 0x02) ? GPIO_PIN_SET : GPIO_PIN_RESET);
 HAL_GPIO_WritePin(GPIOB,r2r_2_Pin,(value & 0x04) ? GPIO_PIN_SET : GPIO_PIN_RESET);
 HAL_GPIO_WritePin(GPIOB,r2r_3_Pin,(value & 0x08) ? GPIO_PIN_SET : GPIO_PIN_RESET);
 HAL_GPIO_WritePin(GPIOB,r2r_4_Pin,(value & 0x10) ? GPIO_PIN_SET : GPIO_PIN_RESET);
 HAL_GPIO_WritePin(GPIOB,r2r_5_Pin,(value & 0x20) ? GPIO_PIN_SET : GPIO_PIN_RESET);
 HAL_GPIO_WritePin(GPIOB,r2r_6_Pin,(value & 0x40) ? GPIO_PIN_SET : GPIO_PIN_RESET);
 HAL_GPIO_WritePin(GPIOB,r2r_7_Pin,(value & 0x80) ? GPIO_PIN_SET : GPIO_PIN_RESET);
}

int _write(int file, char *ptr, int len) {
 HAL_UART_Transmit(&huart2, (uint8_t*)ptr, len, HAL_MAX_DELAY);
 return len;
}

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_TIM2_Init();
 MX_USART2_UART_Init();
 HAL_TIM_Base_Start_IT(&htim2);
 /* USER CODE BEGIN 2 */
 printf("Start\n");
 setFrequency(290);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4;
 RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;
 PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief TIM2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 0;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */
 
 /* USER CODE END TIM2_Init 2 */

}
// Timer interrupt callback
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) {
 static uint32_t sample_index = 0;
 if (htim->Instance == TIM2) {
 output_to_dac(sineLookupTable[sample_index]);
 sample_index = (sample_index + 1) % SINE_TABLE_SIZE;
 HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_0);
 }
}
/**
 * @brief USART2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, r2r_0_Pin|r2r_1_Pin|r2r_3_Pin|r2r_2_Pin
 |r2r_4_Pin|r2r_5_Pin|r2r_6_Pin|r2r_7_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : PA0 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : r2r_0_Pin r2r_1_Pin r2r_3_Pin r2r_2_Pin
 r2r_4_Pin r2r_5_Pin r2r_6_Pin r2r_7_Pin */
 GPIO_InitStruct.Pin = r2r_0_Pin|r2r_1_Pin|r2r_3_Pin|r2r_2_Pin
 |r2r_4_Pin|r2r_5_Pin|r2r_6_Pin|r2r_7_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
    This topic has been closed for replies.
    Best answer by rutvik1110

    Hi everyone, I've managed to complete this task.

    Here is the code:

     

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    TIM_HandleTypeDef htim2;
    
    /* USER CODE BEGIN PV */
    
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_TIM2_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    extern TIM_HandleTypeDef htim2;
    void GPIO_SetValue(uint8_t value) {
    uint16_t pins = 0;
    
     pins |= (value & 0x01) ? r2r_0_Pin : 0;
     pins |= (value & 0x02) ? r2r_1_Pin : 0;
     pins |= (value & 0x04) ? r2r_2_Pin : 0;
     pins |= (value & 0x08) ? r2r_3_Pin : 0;
     pins |= (value & 0x10) ? r2r_4_Pin : 0;
     pins |= (value & 0x20) ? r2r_5_Pin : 0;
     pins |= (value & 0x40) ? r2r_6_Pin : 0;
     pins |= (value & 0x80) ? r2r_7_Pin : 0;
    
     GPIOB->ODR = pins;
    }
    // Function to set new frequency
    void setSineWaveFrequency(uint32_t frequency) {
    
     // Stop Timer 2
     HAL_TIM_Base_Stop_IT(&htim2);
    
     // Recalculate timer period based on new frequency
     uint32_t timer_clock = HAL_RCC_GetPCLK1Freq();
     uint32_t period = timer_clock / (frequency * SINE_TABLE_SIZE);
     
     htim2.Init.Period = period-1;
     HAL_TIM_Base_Init(&htim2);
     
     // Restart Timer 2
     HAL_TIM_Base_Start_IT(&htim2);
    }
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_TIM2_Init();
     /* USER CODE BEGIN 2 */
     TIM2_Config();
     sweep_duration_ms = 5000;
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
     for( int i = START_FREQUENCY ; i<=STOP_FREQUENCY;i++){
     setSineWaveFrequency(i);
     i +=FREQ_STEP;
     HAL_Delay(DELAY_MS);
     }
     HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_0); // Sweep completed
     /* USER CODE BEGIN 3 */
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Configure the main internal regulator output voltage
     */
     __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
     RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4;
     RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief TIM2 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_TIM2_Init(void)
    {
    
     /* USER CODE BEGIN TIM2_Init 0 */
    
     /* USER CODE END TIM2_Init 0 */
    
     TIM_ClockConfigTypeDef sClockSourceConfig = {0};
     TIM_MasterConfigTypeDef sMasterConfig = {0};
    
     /* USER CODE BEGIN TIM2_Init 1 */
    
     /* USER CODE END TIM2_Init 1 */
     htim2.Instance = TIM2;
     htim2.Init.Prescaler = 0;
     htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
     htim2.Init.Period = 65536;
     htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
     htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
     if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
     {
     Error_Handler();
     }
     sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
     if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
     {
     Error_Handler();
     }
     sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
     sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
     if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN TIM2_Init 2 */
    
     /* USER CODE END TIM2_Init 2 */
    
    }
    
    void TIM2_Config(void) {
     __HAL_RCC_TIM2_CLK_ENABLE();
     htim2.Instance = TIM2;
     htim2.Init.Prescaler = 0;
     htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
     htim2.Init.Period = 499; // Default period for 64 kHz
     htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
     if (HAL_TIM_Base_Init(&htim2) != HAL_OK) {
     // Initialization Error
     Error_Handler();
     }
    
     // Enable the TIM2 global Interrupt
     HAL_NVIC_SetPriority(TIM2_IRQn, 0, 1);
     HAL_NVIC_EnableIRQ(TIM2_IRQn);
     
     HAL_TIM_Base_Start_IT(&htim2);
    }
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOB_CLK_ENABLE();
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(GPIOB, r2r_0_Pin|r2r_1_Pin|r2r_3_Pin|r2r_2_Pin
     |r2r_4_Pin|r2r_5_Pin|r2r_6_Pin|r2r_7_Pin, GPIO_PIN_RESET);
    
     /*Configure GPIO pin : PA0 */
     GPIO_InitStruct.Pin = GPIO_PIN_0;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
     /*Configure GPIO pins : r2r_0_Pin r2r_1_Pin r2r_3_Pin r2r_2_Pin
     r2r_4_Pin r2r_5_Pin r2r_6_Pin r2r_7_Pin */
     GPIO_InitStruct.Pin = r2r_0_Pin|r2r_1_Pin|r2r_3_Pin|r2r_2_Pin
     |r2r_4_Pin|r2r_5_Pin|r2r_6_Pin|r2r_7_Pin;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */

    2 replies

    Graduate II
    July 5, 2024

    HAL is not fast and GPIO write in HAL is even slower. Why don't you use  the built-in DAC?

    printf() in the timing critical output routine will also eat up much cycles..

    Visitor II
    July 5, 2024

    I have a R2R network and these bits generate sine waves. I don't know how to do this using built-in DAC, so if you can explain it, I'd be grateful. I have attached my circuit schematics. And printf() was just to debug the value.

    Thanks in advance.

    Graduate II
    July 5, 2024

    For use DAC read examples STM32CubeL0/Projects/NUCLEO-L073RZ at master · STMicroelectronics/STM32CubeL0 · GitHub

    and your code need rewrite 

    void output_to_dac(uint16_t value){
     HAL_GPIO_WritePin(GPIOB,r2r_0_Pin,(value & 0x01) ? GPIO_PIN_SET : GPIO_PIN_RESET);
     HAL_GPIO_WritePin(GPIOB,r2r_1_Pin,(value & 0x02) ? GPIO_PIN_SET : GPIO_PIN_RESET);
     HAL_GPIO_WritePin(GPIOB,r2r_2_Pin,(value & 0x04) ? GPIO_PIN_SET : GPIO_PIN_RESET);
     HAL_GPIO_WritePin(GPIOB,r2r_3_Pin,(value & 0x08) ? GPIO_PIN_SET : GPIO_PIN_RESET);
     HAL_GPIO_WritePin(GPIOB,r2r_4_Pin,(value & 0x10) ? GPIO_PIN_SET : GPIO_PIN_RESET);
     HAL_GPIO_WritePin(GPIOB,r2r_5_Pin,(value & 0x20) ? GPIO_PIN_SET : GPIO_PIN_RESET);
     HAL_GPIO_WritePin(GPIOB,r2r_6_Pin,(value & 0x40) ? GPIO_PIN_SET : GPIO_PIN_RESET);
     HAL_GPIO_WritePin(GPIOB,r2r_7_Pin,(value & 0x80) ? GPIO_PIN_SET : GPIO_PIN_RESET);
    }

    to somethink as

    void output_to_dac(uint8_t value){
    uint16_t temp = GPIOB->ODR & 0xff00;
    GPIOB->ODR |= value;
    }
    rutvik1110AuthorAnswer
    Visitor II
    July 9, 2024

    Hi everyone, I've managed to complete this task.

    Here is the code:

     

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    TIM_HandleTypeDef htim2;
    
    /* USER CODE BEGIN PV */
    
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_TIM2_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    extern TIM_HandleTypeDef htim2;
    void GPIO_SetValue(uint8_t value) {
    uint16_t pins = 0;
    
     pins |= (value & 0x01) ? r2r_0_Pin : 0;
     pins |= (value & 0x02) ? r2r_1_Pin : 0;
     pins |= (value & 0x04) ? r2r_2_Pin : 0;
     pins |= (value & 0x08) ? r2r_3_Pin : 0;
     pins |= (value & 0x10) ? r2r_4_Pin : 0;
     pins |= (value & 0x20) ? r2r_5_Pin : 0;
     pins |= (value & 0x40) ? r2r_6_Pin : 0;
     pins |= (value & 0x80) ? r2r_7_Pin : 0;
    
     GPIOB->ODR = pins;
    }
    // Function to set new frequency
    void setSineWaveFrequency(uint32_t frequency) {
    
     // Stop Timer 2
     HAL_TIM_Base_Stop_IT(&htim2);
    
     // Recalculate timer period based on new frequency
     uint32_t timer_clock = HAL_RCC_GetPCLK1Freq();
     uint32_t period = timer_clock / (frequency * SINE_TABLE_SIZE);
     
     htim2.Init.Period = period-1;
     HAL_TIM_Base_Init(&htim2);
     
     // Restart Timer 2
     HAL_TIM_Base_Start_IT(&htim2);
    }
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_TIM2_Init();
     /* USER CODE BEGIN 2 */
     TIM2_Config();
     sweep_duration_ms = 5000;
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
     for( int i = START_FREQUENCY ; i<=STOP_FREQUENCY;i++){
     setSineWaveFrequency(i);
     i +=FREQ_STEP;
     HAL_Delay(DELAY_MS);
     }
     HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_0); // Sweep completed
     /* USER CODE BEGIN 3 */
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Configure the main internal regulator output voltage
     */
     __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
     RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4;
     RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief TIM2 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_TIM2_Init(void)
    {
    
     /* USER CODE BEGIN TIM2_Init 0 */
    
     /* USER CODE END TIM2_Init 0 */
    
     TIM_ClockConfigTypeDef sClockSourceConfig = {0};
     TIM_MasterConfigTypeDef sMasterConfig = {0};
    
     /* USER CODE BEGIN TIM2_Init 1 */
    
     /* USER CODE END TIM2_Init 1 */
     htim2.Instance = TIM2;
     htim2.Init.Prescaler = 0;
     htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
     htim2.Init.Period = 65536;
     htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
     htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
     if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
     {
     Error_Handler();
     }
     sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
     if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
     {
     Error_Handler();
     }
     sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
     sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
     if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN TIM2_Init 2 */
    
     /* USER CODE END TIM2_Init 2 */
    
    }
    
    void TIM2_Config(void) {
     __HAL_RCC_TIM2_CLK_ENABLE();
     htim2.Instance = TIM2;
     htim2.Init.Prescaler = 0;
     htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
     htim2.Init.Period = 499; // Default period for 64 kHz
     htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
     if (HAL_TIM_Base_Init(&htim2) != HAL_OK) {
     // Initialization Error
     Error_Handler();
     }
    
     // Enable the TIM2 global Interrupt
     HAL_NVIC_SetPriority(TIM2_IRQn, 0, 1);
     HAL_NVIC_EnableIRQ(TIM2_IRQn);
     
     HAL_TIM_Base_Start_IT(&htim2);
    }
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOB_CLK_ENABLE();
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(GPIOB, r2r_0_Pin|r2r_1_Pin|r2r_3_Pin|r2r_2_Pin
     |r2r_4_Pin|r2r_5_Pin|r2r_6_Pin|r2r_7_Pin, GPIO_PIN_RESET);
    
     /*Configure GPIO pin : PA0 */
     GPIO_InitStruct.Pin = GPIO_PIN_0;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
     /*Configure GPIO pins : r2r_0_Pin r2r_1_Pin r2r_3_Pin r2r_2_Pin
     r2r_4_Pin r2r_5_Pin r2r_6_Pin r2r_7_Pin */
     GPIO_InitStruct.Pin = r2r_0_Pin|r2r_1_Pin|r2r_3_Pin|r2r_2_Pin
     |r2r_4_Pin|r2r_5_Pin|r2r_6_Pin|r2r_7_Pin;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */