New Ethernet driver does not work properly (F4 series)
Guys, unfortunately I don't know what to do. A few days ago I updated to the latest HAL version for the F4 series (1.8.3). With 1.8.0 there was a big change in the Ethernet driver, so some adjustments were necessary. I already used the low_level_...() functions from ST, which are included in the examples and are also generated by CubeMX.
Since the upgrade I always get DMA errors in the function HAL_ETH_Transmit(). More precisely at the following point:
/* Wait for data to be transmitted or timeout occurred */
while ((dmatxdesc->DESC0 & ETH_DMATXDESC_OWN) != (uint32_t)RESET)
{
if ((heth->Instance->DMASR & ETH_DMASR_FBES) ! = (uint32_t)RESET)
{
heth->ErrorCode |= HAL_ETH_ERROR_DMA;
heth->DMAErrorCode = heth->Instance->DMASR;
/* Return function status */
return HAL_ERROR;
}
[..]heth->DMAErrorCode then contains the following value: 0x1886486
The strange thing is, simple pings, UDP and TCP echo servers work. However, as soon as the amount of data increases (http), the function exits with HAL_ERROR.
I also had a look at the parameters passed to the function low_level_output(struct netif *netif, struct pbuf *p), especially the *p variable and compared it with the old, working driver version. The content of *p is completely identical. There are 5 chained buffers. Both the content and the memory addresses are identical with the old and new driver versions. Ping and Co work because only one pbuf is allocated here.
I have now also created a new CubeMX project where only Ethernet is configured with LwIP. Here the same thing happens with the same error code in heth->DMAErrorCode.
Has anyone got the new Ethernet driver running on an F407? Any ideas?