New to STM - is there a clear best choice board for real-time audio & video programming / possibly ML?
I've been recommended the G4 or F3 based just on the fact that I'm interested in DSP, but am still trying to narrow things down a bit further, or get a second opinion.
One particular project I'm especially interested in is a live audio sampler / looper, so I either need on-board ADCs/DACs or an I2S interface (I have a PMOD I2S2, so as long as I can hook that up). I would also like a board that is very little interrupt latency since this project would involve a lot of starting / stopping / manipulating signals on the fly. I highly doubt any of the boards have enough on-board memory that I can store substantial audio samples, so I'd probably need an off-board RAM and an easy way to connect to that.
In general, I like plenty of freedom with programming boards and very little hardware abstraction. I don't know if that makes a difference.
Sorry if all of these specs are trivial, and maybe any board will do, but I thought I would ask the community!