no IOC file for a published U585i-IOT02a example?
Given that it is very easy to cause signal conflicts when configuring an MCU using the CubeMX initialization program, it is extremely important to include the IOC file for any particular example published. This being for comparison when trying to use an example as a base and extrapolate additional functionality. Since the CubeMX program is cryptic about about signal conflicts, being able to inspect the IOC is the only/best way to quickly determine how things are set up. Also, it is needed if using the example project as a base for further experimentation.
U585i-IOT02A BSP example does NOT contain the IOC file used to initialize the MCU for the project.