No response from CAN Bootloader -> STM32L496 (Nucleo)
Hello,
i would like to do firmware upload via CAN bus on my STM32L496 (Nucleo) board.
According to the datasheet this chip support firmware update via CAN.
I have a working CAN setup, i am able to send and recieve CAN frames, so i think the hardware side is okay.
After reboot into bootloader (BOOT0 == high) i am not able to get any response from the bootloader. According to the AN3154 i tried a few commands without any response.
I am able to reach the bootloader via UART and USB without any problems.
are the any tips and tricks with that?
thanks
Max