Non blocking SPI DMA transceive never completes in RTOS application
Description:
My RTOS application on NUCLEO-H563ZI board runs a thread CollectSamplesThread. I generate an interrupt every 8Khz using a timer and the ISR triggers a non blocking SPI transfer:
The application code:
void InitAdeSpi()
{
// SPI1 Initialisation
if (hSPI.hdmarx != NULL)
{
HAL_DMA_RegisterCallback(hSPI.hdmarx, HAL_DMA_XFER_CPLT_CB_ID, AdcSpiRxCallback);
}
}
void AdcSpiRxCallback()
{
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
// Release the sempahore thats blocked to validate the frames in CollectSamplesThread
xSemaphoreGiveFromISR(xSpiRxSemph, &xHigherPriorityTaskWoken);
portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}void TIM3_IRQHandler(void)
{
EvbDataRdyTimerHandler();
}
void EvbDataRdyTimerHandler(void) // Ensure this matches the existing declaration
{
__HAL_TIM_CLEAR_FLAG(&hTimDready, TIM_FLAG_UPDATE);
// Release the sempahore that is blocked in the CollectSamplesThread for Dready callback
xSemaphoreGiveFromISR(xSamplesAvailSemph, &xHigherPriorityTaskWoken);
portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
} void CollectSamplesThread(void *pArg)
{
HAL_StatusTypeDef halStatus;
int32_t status = 0;
if (pArg == NULL)
{
while (1)
{
if (xSemaphoreTake(xSamplesAvailSemph, portMAX_DELAY) == pdTRUE)
{
halStatus = HAL_SPI_TransmitReceive_DMA(hSPI, pTxData, pRxData, (uint16_t)numBytes);
if (halStatus != HAL_OK)
{
status = -1;
}
if (status == 0)
{
if (xSemaphoreTake(xSpiRxSemph, portMAX_DELAY) == pdTRUE)
{
//Validate samples
}
}
}
}
}Issue:
Tx DMA ISR is hit, Rx DMA ISR is not hit. SPI1 ISR, SPI1_IRQHandler, is also not hit.
Additional info:
System clock is configured to 250 Mhz.
Before calling HAL_SPI_TransmitReceive_DMA,
- SPI1->SR = 0x00011002 (TXP=1, TXC=1, no EOT)
- SPI1->IER = 0x0 (interrupts disabled)
At if (halStatus != HAL_OK),
- SPI1->SR = 0x00010012 (TXP=1, EOT=1, TXC=1) ✓ EOT flag is set
- SPI1->IER = 0x00000360 (EOTIE=1, bits 5,6,8,9 enabled) ✓ EOT interrupt is enabled