Skip to main content
Visitor II
October 24, 2022
Question

Not able to connect to WiFi during the STM32L4 Discovery kit IoT node Getting Started

  • October 24, 2022
  • 4 replies
  • 2046 views

Hi,

I'm trying to run the Getting Started firmware for the B-L475E-IOT01A board but I'm having problems to connect to WiFi. The error messages are:

"ERROR: C:\STM32CubeExpansion_Cloud_AWS_V1.4.1\Middlewares\ST\STM32_Connect_Library\core\net_core.c:327 Interface cannot be connected

ERROR: platform_init L#254 Unable to connect netif"

0693W00000UocS8QAJ.png 

These are my WiFi Properties:

0693W00000UocT1QAJ.png 

OBS:

  1. I'm using the following Getting Started firmware: STM32CubeExpansion_Cloud_AWS_V1.4.1\Projects\B-L475E-IOT01A\Applications\Cloud\AWS\Binary\SBSFU_B-L475E-IOT01_Cloud_AWS_V1.4.1.bin
  2. The target board is the B-L475E-IOT01A2

Am I missing something?

Thanks in advance,

Guilherme Amorim.

    This topic has been closed for replies.

    4 replies

    Technical Moderator
    October 24, 2022

    Hello @gvamorim​ and welcome to the Community :)

    Did you try the WiFi project for B-L475E-IOT01A board available within STM32CubeL4 MCU package?

    Imen

    ST Employee
    October 24, 2022

    hello.

    • are you using an iPhone as WiFi/4G gateway to connect the B-L475E-IOT01 to WiFi ? with a recent version of iOS ? it may require WPA3 which B-L475E-IOT01 WiFi module doesn't support.
    • other possibility (maybe): try to configure the SSID name of your WiFi access point without a space character in the SSID name
    gvamorimAuthor
    Visitor II
    October 25, 2022

    Hi @Guillaume K​ and @Imen DAHMEN​ ,

    I'm now able to connect to the WiFi access point. It seems that the WiFi should be configured with access point and I was not aware of that.

    Thanks a lot,

    Guilherme Amorim.

    ST Employee
    October 25, 2022

    Hello,

    what was the configuration of your Wifi if it was not access point ?

    Guillaume