NUCLEO F429ZI board - Ethernet over usb - zperf example communication issue
I need help running the zerpf example with USB over ethernet for the STM32 NUCLEO F429ZI board. I could run the example with an ethernet port and ping the connection using iperf-2.0.5b-win32.
However, when I have configured the proj.conf file by adding these lines for setting Ethernet over USB.
CONFIG_USB_DEVICE_STACK=y CONFIG_USB_DEVICE_NETWORK_ECM=n CONFIG_USB_DEVICE_NETWORK=y CONFIG_USB_DEVICE_NETWORK_RNDIS=y CONFIG_NET_IPV6=n #Disabled this flag else mcu reboot again and again when the command is sent)
These configuration settings are also described here: sample.net.zperf.netusb_rndis After flashing the code, an RNDIS network is discovered via a USB connection, and I can manually set the network's IP. However, when I run iperf-2.0.5b-win32 in server mode on my Windows 11 and send zperf tcp upload 192.0.2.2 5001 10 1K 1M on the board, I get the error.
TCP upload failed (-116)
The connection is not established for TCP. Also, I am getting an error for UDP upload failed (-115). Can anyone help me understand what the problem might be?