NUCLEO-H7S3L8 USB_HS Clock Reset Timeout
The USB_OTG_HS peripheral keeps timing out on init and hanging the whole program.
I have created a STM32 project using the NUCLEO-H7S3L8 board from the new project menu. I have enabled the USB_OTG_HS as device only (but left the middleware disabled) and written a simple blinky main. The code always times out on the "MX_USB_OTG_HS_PCD_Init". Specifically USB_CoreReset() times out in "stm32h7rsxx>USB_CoreInit". I have tried multiple different USB clock configurations (HSE, HSE/2 and PLL3Q) but it still times out.
Some people have suggested (Solved: STM32U595 timeout in USB_CoreReset() - STMicroelectronics Community) including the below in "HAL_PCD_MspInit" but STMCube cannot find it and I can't where to include it from
_HAL_RCC_SYSCFG_CLK_ENABLE();
I have included my project.zip but it is just the board default project. I have XSPI1, XSPI2 and ExternalMemLoader disabledExternal disabled., And have enabled the High-Speed Crystal/Ceramic Resonator, the blue LED and the USB_OTG_HS as device only.
I'm really struggling to find a way forward, I would appreciate any guidance.