Nucleo-H7S3L8 with RTOS: HAL_IncTick() always returning 0
Hi everyone,
I'm working on an STM32H7RS project (NUCLEO-H7S3L8) with the following setup:
Bootloader in internal flash (0x08000000)
Application in external OSPI flash (XIP) at 0x70000000
Using Azure RTOS (ThreadX)
Using TIM6 as the HAL time base (not SysTick)
Configured using latest STM32CubeMX and STM32CubeIDE (v1.18.1)
What I already checked:
The vector table is correctly set in main() of the application:
int main(void)
{
/* USER CODE BEGIN 1 */
#define APPLICATION_VECTOR_TABLE ((uint32_t)0x70000000)
SCB->VTOR = APPLICATION_VECTOR_TABLE;
__DSB();
__ISB();
/* USER CODE END 1 */
/* Enable the CPU Cache */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
/* MCU Configuration--------------------------------------------------------*/
/* Update SystemCoreClock variable according to RCC registers values. */
SystemCoreClockUpdate();
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_HPDMA1_Init();
MX_GPDMA1_Init();
uint32_t tickTest3 = HAL_GetTick();
MX_ADC1_Init();
MX_ADC2_Init();
MX_I2C2_Init();
MX_SBS_Init();
MX_UART4_Init();
MX_UART5_Init();
MX_TIM3_Init();
MX_TIM2_Init();
MX_UART7_Init();
MX_UART8_Init();
MX_I2C3_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_ETH_Init();
MX_FLASH_Init();
MX_DTS_Init();
MX_TIM1_Init();
/* USER CODE BEGIN 2 */
/* Initialize leds */
BSP_LED_Init(LED_GREEN);
BSP_LED_Init(LED_BLUE);
BSP_LED_Init(LED_RED);
/* USER CODE BEGIN BSP */
/* -- Sample board code to send message over COM1 port ---- */
printf("Welcome to STM32 world !\n\rApplication project is running...\n\r");
/* -- Sample board code to switch on leds ---- */
BSP_LED_On(LED_GREEN);
BSP_LED_On(LED_BLUE);
BSP_LED_On(LED_RED);
/* USER CODE END BSP */
/* USER CODE END 2 */
MX_ThreadX_Init();HAL_Init() is called before anything else
HAL_InitTick() has been overridden to use TIM6
HAL_TIM_Base_Start_IT() returns HAL_OK
TIM6_DAC_IRQHandler() is defined and includes a call to HAL_IncTick() via HAL_TIM_IRQHandler()
- HAL_TIM_PeriodElapsedCallback() is implemented and includes:
if (htim->Instance == TIM6) {
HAL_IncTick();
}
The TIM6 interrupt priority is set to 14, and NVIC config is applied
uwTick remains at 0 the entire time — HAL_GetTick() and HAL_Delay() don’t function
MX_Eth_Init works, indicating that clocks, NVIC, and system init are not completely broken
Using the default ThreadX integration generated by STM32CubeMX for Azure RTOS
I also upleaded my IOC file. Are there any known issues or things i have overseen?