NucleoF303RE PWM on TIM3 (PA6) Not Working – No Output Signal
I am working with an STM32F303 and trying to generate a PWM signal on TIM3, Channel 1 (PA6). Everything seems to be correctly configured (verified in the debugger – registers appear correct), but there is no PWM signal on PA6. The function responsible for clock configuration worked correctly in the case of USART. In the IRQ handler, the flag registers are set correctly, which I verified using a breakpoint. I would appreciate any help in identifying the possible cause of why the PWM is not activating.
void configureTIMER3(void)
{
//PA6:D12
RCC -> APB1ENR |= RCC_APB1ENR_TIM3EN;
TIM3->PSC = 711; //72mghz
TIM3->ARR = 99; //PA6
}
void clock_config(void)
{
RCC->CR |= RCC_CR_HSION;
while (!(RCC->CR & RCC_CR_HSIRDY));
RCC->AHBENR |= RCC_AHBENR_GPIOAEN;
RCC->APB1ENR |= RCC_APB1ENR_PWREN;
// FLASH -> ACR = FLASH_ACR_PRFTBE | FLASH_ACR_PRFTBS | FLASH_ACR_LATENCY_2;
RCC->CFGR |= RCC_CFGR_HPRE_DIV1;
RCC->CFGR|= RCC_CFGR_PPRE1_DIV2;
//PPL SOURCE MUX
// RCC->CFGR |= RCC_CFGR_PLLMUL9;
RCC->CFGR |= (0x7 << RCC_CFGR_PLLMUL_Pos);
RCC->CR |= RCC_CR_PLLON;
while (!(RCC->CR & RCC_CR_PLLRDY));
RCC->CFGR |= RCC_CFGR_SW_PLL;
while(!(RCC->CFGR & RCC_CFGR_SWS));
}
void TIM3_start(void)
{
TIM3->CNT=0;
TIM3->CR1|= TIM_CR1_CEN;
}
void interuptTIM3(void)
{
TIM3 -> DIER |= TIM_DIER_UIE;
TIM3 -> DIER |= TIM_DIER_CC1IE;
NVIC_SetPriority(TIM3_IRQn, 0);
NVIC_EnableIRQ(TIM3_IRQn);
}
void TIM3_IRQHandler(void)
{
if(TIM3 -> SR & TIM_SR_UIF)
{
TIM3 -> SR &= ~(TIM_SR_UIF);
}
if(TIM3 -> SR & TIM_SR_CC1IF)
{
TIM3 -> SR &= ~(TIM_SR_CC1IF);
}
}
void pwmconfigration(void)
{
TIM3 -> CCMR1 |= TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2;
TIM3 -> CCMR1 |= TIM_CCMR1_OC1PE;
TIM3 -> CCR1 = 49;
TIM3->CR1 |= TIM_CR1_ARPE;
TIM3 -> CCER |= TIM_CCER_CC1E;
}
void configPWMPA6(void)
{
GPIOA-> MODER |= GPIO_MODER_MODER6_1;
GPIOA->AFR[0] |= (0x2 << GPIO_AFRL_AFRL2_Pos);
}
int main(void)
{
//SysTick_Config((72000000/ 1000));
//configPWMPA6();
clock_config();
configureTIMER3();
pwmconfigration();
configPWMPA6();
TIM3_start();
interuptTIM3();
//1s = 72 000 000
// 0,001 = x
/* Loop forever */
while(1)
{
}
}