Nx_TCP_Echo_Server with static IP
Hello,
I need the TCP Server with static IP address. I chose the Nx_TCP_Echo_Echo_Server example and NUCLEO-H723ZG board as a starting point. I use the STM32CubeIDE 1.19 with latest x-cube-azrtos-h7-v3-4-0 sample files. So I imported the Nx_TCP_Echo_Echo_Server example project and compiled it without problems. But after that I disabled DHCP and set the static IP address:
After that project can't be build and it is necessary to edit app_netxduo.c file as in it still there are some code related to DHCP. But even after successful compilation I can't connect to the server from the client. Also I can't ping it too.
It seems that this is a global problem with NetXDuo as there are plenty of posts with similar problems. E.g.:
https://community.st.com/t5/stm32-mcus-embedded-software/netxduo-not-working-with-a-static-ip-addresss/td-p/673975
https://community.st.com/t5/stm32-mcus-embedded-software/http-server-on-netx-and-azrtos-disable-dhcp-when-using-fixed-ip/td-p/94729
I've tried to implement all the recommendations from these posts, but still no result.
I attach my project and raise the question - how the TCP server with Static IP address can be realized using NetXDuo ?
- on