Skip to main content
Graduate II
May 29, 2025
Solved

PA0_C/PA1_C/PC2_C/PC3_C[STM32H743XGH6]

  • May 29, 2025
  • 1 reply
  • 333 views

PA0_C/PA1_C/PC2_C/PC3_C
What is the base address for the above four GPIOs that can be set?

Also, do you have the following understanding about the above 4 pins?
Pxy_C can be set to a pin of the same function or another function by controlling an analog switch.

    This topic has been closed for replies.

    1 reply

    NiMAuthor
    Graduate II
    June 11, 2025

    Thank you very much.

    I understand, there is no separate configuration register for Pxy_C, you are talking about whether or not it is connected via a switch to the Pxy's pins.