[Please ignore] STM32U5, ThreadX and CMSIS
[EDIT: S'OK, I need to think about this more, but I can't find a way to delete a message so am just marking this as one to ignore]
I am just moving from STM32F4 to STM32U5. ThreadX seems to be the thing for STM32U5 (if one doesn't want to use Zephyr) but I need to be able to use FreeRTOS also, so I have moved all of my code to CMSIS (V2). However, I am not able to find cmsis_os.h/cmsis_os2.h for ThreadX. For instance, in the STM32F4 case the CMSIS API for FreeRTOS can be found under the Middlewares/Third_Party/FreeRTOS/Source directory.
The STM32CubeU5 only contains "template" cmsis_os.h/cmsis_os2.h files but I don't want a template of my RTOS interface, I want the actual RTOS interface that ThreadX will abide by. The cmsis_rtos_threadx directory of STM32CubeU5 only contains the .c file, no headers. The ThreadX repo doesn't contain a CMSIS adaptation at all.
Where do I find the CMSIS adaptation API that ThreadX will abide by?