Please suggest a SIL2 Certified 32-bit Micro Controller.
We are working on Redesign activity of a PLC System; In that we have to Replace Micro controller. Could you please suggest a Low-cost and Sil2 Certified 8,32-bit Micro controller .
Requirement:
1.SIL2 Certified controller
2.48 or More Pin's, SPI Interface - 01 + 01(Optional)
3. SIL Related libraries should be support
4.1K bytes of ram, 1K bytes of eeprom and 12k of on-chip rom(Minimum).
5. Clock frequency >3 MHz
6. Operating Temperature -40°C to +85°C
7. Operating Voltage 3V to 5.5V
Please let me know if you have any questions.