PLL: anybody using the internal PLLs as VCO for audio?
Hello,
I was just porting a F767 design to an H723-Nucleo, and found out that this H7 Nucleo is using its ST-Link's HSI as a clock source to the H723 at 8 MHz. With the usual terrible HSI quality, which showed itself in low quality SPDIF TX and PTP sync.
So I switched the ST-Link's clock to HSE output, which changed the frequency to 8.333 MHz, which again led me to using the FRACN registers for the first time to get some even clock numbers.
I also found that the FRACN values can be changed on the fly, which might let me save an external VCO (which until now I controlled with the 12bit DAC).
So, has anybody ever used the internal PLL's FRACN for syncing and sourcing audio stuff?
If yes, how was the quality (jitter while changing FRACN)?