Skip to main content
Visitor II
November 17, 2021
Solved

Porting Azure RTOS examples

  • November 17, 2021
  • 1 reply
  • 893 views

Hi, last time I ported an Azure RTOS project there were only a handful of BSPs so I had to do some manual fiddling around to get it running on a nucleo board. Now that there is full support for H7 processors in the 2.0 package I'm wondering what the best steps to move a project over would be.

I imagine I can start a new project in CubeMX and then "import" the ioc file, generate the base project and then copy in the source code - but wondering if there is a cleaner way of doing it.

TIA, Oliver

    This topic has been closed for replies.
    Best answer by STM32_ZA

    Hi,

    As you said you need to generate a new project for target board/MCU first then :

    1-configure the HW IPs (GPIO, System clock, ETH, USB,,..)

    2- Enable/Configure the components of Azure RTOS pack

    3- Generate project and copy application source code from an existing example into your new project 

    1 reply

    STM32_ZAAnswer
    ST Employee
    November 18, 2021

    Hi,

    As you said you need to generate a new project for target board/MCU first then :

    1-configure the HW IPs (GPIO, System clock, ETH, USB,,..)

    2- Enable/Configure the components of Azure RTOS pack

    3- Generate project and copy application source code from an existing example into your new project