Position Independent Code
Hello
I am trying to merge USB CDC code into an existing code which is a Keil multi project code. I am using the USB CDC code generated by stm32cubemx for data transmission and reception testing.
The multi project is position independent build and when i add the files from USB CDC test application into it, it throws following errors and warnings. I am new to PI concept and would really appreciate if someone could guide me over this and help me resolve these.
Thanks.
*********************************************
*** Using Compiler 'V5.06 update 4 (build 422)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
WARNING: usbd_cdc_if.c(150): warning: #1357-D: static initialisation of variable "USBD_Interface_fops_FS" using address of CDC_Init_FS may cause link failure -ropi
USBD_CDC_ItfTypeDef USBD_Interface_fops_FS =
linking...
.\objects\zero.axf: Error: L6248E: usbd_cdc.o(.data) in PI region 'ER_RW' cannot have address type relocation to USBD_CDC_Init in PI region 'ER_RO'.
*********************************************