Preciserr hardfault at random times, when using lwip and ethernet
Hi, I am developing a project with an STM32H7 microcontroller, that has to do with ethernet connectivity. More specifically it is an embedded display that runs freeRTOS v2 code, which is being generated automatically from touchGFX. I used the cubemx in order to enable the ethernet peripheral, the LwIP to assign a static IP address to my board, and also I set MPU configurations. After that, when I generate my code, I set a section into the linker script file (lwip_sec) and set the DMA descriptors to run in RAM_D2 also with the RX_pool buffer. I manage to succeed to work with the peripheral I can ping my board correctly, although at a random time it generates a precise hardfault error. So I would like to ask a question about linkerscript. Is there any additional process that it needs to be done in linkerscript (for example, change the length of ram or other things, when a new section is being initialized) in order to avoid the hardfault error, or it isn't related the linkerscript with that error?
I have followed the same steps like this video: https://www.youtube.com/watch?v=sQ3rgQNGKV4, with the only difference is that I work with touchgfx but the video has the lvgl library.