Problem entering the bootloader using the STM32H753 and pattern 8
We are using the STM32H753 and cannot enter the bootloader using pattern 8.
AN2606 states that when BOOT0 is low and the option byte BOOT_ADD0 is 0x0040, then the bootloader is activated.
Does this work for the STM32H753?
Pattern 8
Option byte set to 0x0040 in STM32CubeProgrammer
Thanks for your help!