Skip to main content
Visitor II
April 7, 2021
Question

Problem in Integrating SPI module in Tx_CMSIS_Wrapper example project

  • April 7, 2021
  • 2 replies
  • 708 views

Hi,

I

have downloaded an example (Tx_CMSIS_Wrapper) project for stm32h747 discovery

kit from STM32CubeMX. After downloading the example project, I was able to

compile it on STM32CubeIDE 1.6.0 and flash it in the board. I was able to

program both the cores and run it individually.

After

this, I wanted to add a SPI interface in the same example project. For this, I

uncommented #define HAL_SPI_MODULE_ENABLED in stm32h7xx_hal_conf.h in both of

the cores and after that I called the MX_SPI1_Init function main.c file. While

calling the initialisation function in main.c file, it was able to locate

stm32h7xx_hal_spi.h file but it could not find stm32h7xx_hal_spi.c file.

It

was showing the error undefined

reference to `HAL_SPI_Init' while building.

I

checked the folder structure of STM32H7xx_HAL_Driver folder and the file stm32h7xx_hal_spi.c is available in the folder

structure. The folder structure is already included in the path and USE_HAL_DRIVER is also available in the setting. So, I don't

know where the problem is and I am stuck in it.

The program compiles all other

modules that came with the example project however it does not compile the

module that I have added later in the project.

Could you please help me out with

this problem?

    This topic has been closed for replies.

    2 replies

    Visitor II
    April 26, 2021

    In which package spi flash program,you got

    Super User
    April 26, 2021

    Make sure that SPI is enabled in your stm32h7xx_hal_conf.h