Problem in UART INTERRUPT call back function
Hey guys!
I am currently working on stm32F2 series, the issue i was facing in HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) when the UART transmit the first byte the interrupt call back function is not called instead calling the RxCpltCallback it call the " USART1_IRQHandler(void) "and the RxCpltCallback function does not trigger at first byte in UART at the second byte it call the RxCpltCallback function and it works fine and i attached the code i was wrote
#include "main.h"
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart3;
unsigned char ra_buffer[32];
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART3_UART_Init(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_USART3_UART_Init();
HAL_UART_Receive_IT(&huart1,ra_buffer,12);
while (1)
{
HAL_Delay(1000);
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Receive_IT(&huart1,ra_buffer,1);
HAL_UART_Transmit(&huart3,ra_buffer, 1,100);
}