Problem using 'NUCLEO-G0B1RE' with USB Host CDC class
I'm trying to communicate with an external device with a USB-C Device interface in CDC Serial class.
I'm following the steps as shown in the video
However, in my debugging, I cannot access the 'userFunction();' function."
void userFunction(void)
{
static uint32_t i = 0;
static uint8_t init_receive = 0;
if(Appli_state == APPLICATION_READY)
{
if(init_receive == 0){
USBH_CDC_Receive(&hUsbHostFS, rx_buffer, 9);
init_receive = 1;
}
if((HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13) == GPIO_PIN_SET) && i>0XFFFF)
{
USBH_CDC_Transmit (&hUsbHostFS, tx_buffer, 9);
i=0;
}
i++;
}
}
Appli_state is always at '0' (APPLICATION_IDLE).
Can someone help me with this issue?
I'm attaching files that might help with the analysis
Thanks in advance!