Problem when change delai of a synced timer
Hello Forum,
I am struggling with a sync timer problem and I have no more idea for resolve it. Here we go :
TMR5 is configured as master for TMR3
TMR3 is configured as master for TMR4
I configured TMR3 as OnePulse output signal with a delai from a OutputCompareStatus of TMR5
I configured TMR4 as PWM signal started by OutputCompareStatus of TMR3
I do Init/Configure/Start after a powerOn and the system works well. I want to do an update of the delai on TMR3 and, impossible to have a correct synchronization between my signals as in the first call.
I did several attempt and I lost my self in all theses, someone know the exact sequence of call I have to do for make the magic happened ?
Thanks a lot
When it works,

Any other attempt stop/update same delai/start, the blue wave loose the synchro

Mickael