Skip to main content
Visitor II
May 10, 2022
Question

Problem with application, after booting from mcuboot.

  • May 10, 2022
  • 1 reply
  • 981 views

Hello All,

I'm trying to chain load the baremetal application from mcuboot with stm32f429. It's chainload the application and reaches the baremetal main function but even though there is some problem with clock configuration, the application went to unknown state after after clock configuration. What is the proper way the transfer control to application from bootloader.

Right now, before handovering the control to application, I properly de initialized the clock, hal and systick timer. Below is the code snippet

 __disable_irq();
 SysTick->CTRL =0;
 SysTick->LOAD=0;
 SysTick->VAL=0;
 HAL_RCC_DeInit();
 HAL_DeInit();

And what is the best way to debug the mcuboot and application together with gdb?

    This topic has been closed for replies.

    1 reply

    Graduate II
    May 10, 2022

    Does anyone of your code enable the interrupts again?​

    I​f you creates some contractual obligations between stages you don't need to teardown the clocks only to reinitialize them.

    A​ debugger should be able to step through the transition, even if only at a disassembly level.