Problem with RX OVERRUN when using SD card DMA
I have an STM32H745 board and I am trying to use FatFS, SDIO, FreeRTOS and DMA.
I know this is a mix fraught with difficulties based on all the posts I have seen and all the things I have tried.
I have it working without DMA ... but it is flakey.
So I wanted to move to DMA but every attempt fails with the HAL_SD_ERROR_RX_OVERRUN error returned by the HAL_SD_IRQHandler(&hsd1) call.
This is failing before FreeRTOS even kicks in ... so I dont think that is a factor.
Reading suggests adding hardware flow control or slowing down the clock by increasing the clock divider ... but nothing seems to help.
This is my SDMMC initialisation code:
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
hsd1.Init.ClockDiv = 128;
HAL_StatusTypeDef err = HAL_SD_Init(&hsd1);
HAL_NVIC_SetPriority(SDMMC1_IRQn, 0x01, 0);
HAL_NVIC_EnableIRQ(SDMMC1_IRQn);
If i set the priority to a larger number the interrupt stops firing ... i dont really understand why but that will be a follow up question as that will be important to make it work well once the RTOS is running.
This is the code that actually kicks off the DMA read ...
if (BSP_SD_ReadBlocks_DMA((uint32_t*)alignedBuffer,
(uint32_t)(sector),
count) == MSD_OK)
{
timeout = HAL_GetTick();
while ((readStatus == 0) && ((HAL_GetTick() - timeout) < SD_TIMEOUT)) {
}
if (sdErr == 0 && readStatus == 0) {
SendDebug(" SD Card read timeout.\r\n");
Global_Error_Handler();
return RES_ERROR;
}
if (sdErr != 0) {
// this is where i end up because my DMA error handler is called
DebugSDCode(sdErr);
return RES_ERROR;
}
// at this point it is of course a success
...
This is my DMA error handler which gets called
void HAL_SD_ErrorCallback(SD_HandleTypeDef* hsd)
{
sdErr = hsd->ErrorCode;
}
and my read complete which doesnt
void BSP_SD_ReadCpltCallback(void)
{
readStatus = 1;
}
At this point i will take any hints anyone might have.
If I have missed anything you might need to see please just ask.