Project with own bootloader goes into "b Infinite_Loop" when an timer interrupt occure.
Hi,
i have written a custom bootloader + end user application for STM32G030K8.
When i run the bootloader seperately , then the bootload code works as expected
When i run the user application from addres 0x0800000 then the code works fine.
But after i make the changes to be able to build and debug bootloader + enduser application, some things go wrong...
- changes made are
1) in end user applications system_stm32g0xx.c , i have changed the vect tab offset
#define VECT_TAB_OFFSET 0x00005800U
2) in end user applications STM32G030K8TX_FLASH.ld , i have changed the origin FLASH (rx) : ORIGIN = 0x8005800, LENGTH = 40K
3) in bootloader applications STM32G030K8TX_FLASH.ld , i have changed the length
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 22K
(2 k is used to write data to flash)
- in debug settings
when i run the debugger with above settings , the debugger starts at in main(void) from the end user application? I expect the debugger would start in main of the bootloader.
But when i press the reset chip button,
then the debugger jumps to the first line of the bootloader (as expected).
At this point the debugger start running the bootload program, and jumps to the end user main loop as designed, so the bootloader does what i need to do.
In the end user application main loop i can step everything until the first timer 16 interrupt is fired, when that happens then the code is running in the b infinite_loop...
/**
* @brief This is the code that gets called when the processor receives an
* unexpected interrupt. This simply enters an infinite loop, preserving
* the system state for examination by a debugger.
*
* @param None
* @retval None
*/
.section .text.Default_Handler,"ax",%progbits
Default_Handler:
Infinite_Loop:
b Infinite_Loop
.size Default_Handler, .-Default_HandlerIt seems that the interrupt vector is at a wrong address . what did i miss?
Thank you