PWM register of TIMER
I have initialized a project with STM32CubeIDE (the .ioc file) using the STM32F407G discovery.
I want to produce on an output pin of the TIMER4 a PWM signal with a certain duty cycle, so I set in the .ioc file the various parameters and in particular the "Pulse" parameter which, if I am not wrong, takes values in the range [0 .. ARR]. The value 0 corresponds to 0% Duty Cycle while the value ARR corresponds to 100% Duty Cycle. Is this correct?
Since I want to be able to change the pulse parameter dynamically without having to set it every time by opening the .ioc file ... I decided in the main.c to directly change the register responsible for the Pulse parameter. So in the Reference Manual I looked up what it was and I found "one pulse mode" (in the attached reference manual, see section 18.3.10). I have read it several times but I can't figure out which register stores the Pulse value of TIMER4.
I found out "indirectly" that it's CCR3 register because, during the simulation/debug, in the SFRs section I saw that in CCR3 there was a decimal value equal to the one set in "Pulse" in the .ioc file
Can you help me understand that CCR3 is the Pulse register only by using the documentation? (datasheet, reference manual, etc.)

Thanks!