QSPI is not working on STM32H747 in FreeRTOS thread
Title edited by a ST moderator to reflect the content.
Hello,
STM32CubeMX Version:6.15.0
STM32CubeH7 Firmware Package V1.12.0 / 30-October-2024
This Is My QSPI Configure in STM32CubeMX

1、When I Start QSPI Work in main function,The QSPI Will always work。QSPI work on CM4-Core。
source:

The QSPI CS signal wave,which Delta Time is 13us,not big than 1s according code:

2、When I Start QSPI Work in FreeRTOS Thread,The QSPI-CS signal Always High,and clock is always out 。QSPI work on CM4-Core。
source:

The CS Signal is always High, And clock signal is always output.The next is qspi-clock signal:

My Question is:
1、When I Start QSPI transmit-receive in main() function, It will always work, no stop. It's CS-signal always output low and high. Why?
2、When I Start QSPI transmit-receive in FreeRTOS thread, It does not work, CS-signal is always High, and clock is always output.
I Have No Idea to solve it after many trial, Could You Have Some Idea?