Skip to main content
Explorer
May 19, 2023
Question

Query on class b for STM32U585 Controller

  • May 19, 2023
  • 2 replies
  • 1315 views

Hello Support Team,

Have a wonderful day.

We are selected Trustzone MCU STM32U585ZIT6Q for our product we have some queries regarding the certification

Based on the attached user guide snapshot, we could understand this U5 series chip have a Class B library that supports IEC 61518 and was adopted to fulfil the IEC60730 requirement.

Is that ok to proceed with UL1998/IEC60730 certification by integrating the ClassB STL library for the U5 series?

Also, could you share the latest UL-compliant certificate for the STM32 U5 series?

Thanks

Hiren R. Thumar


_legacyfs_online_stmicro_images_0693W00000bkRDMQA2.png

    This topic has been closed for replies.

    2 replies

    Explorer
    May 26, 2023

    Hello Support team,

    Have a good day.

    we have found the UL/IEC60703 certification for the STM32U5 series below the link

    https://www.st.com/resource/en/certification_document/e480533-20220630-certificateofcompliance.pdf

    But we have some queries which I mentioned below

    1. How to run class B library code in a secure region (can I establish a timer ISR and access the class B lib API in ISR Routine? )Please share examples with us if you have any.

    2. if we do not enable a trust zone so can I use the same MCU as the non-secure region, also can we able to use dual bank and SBSFU functionality(In Disble trust zone configuration)?

    Thanks & Regards

    Hiren R. Thumar

    ST Employee
    May 29, 2023

    X-CUBE-CLASSB for STM32U5 series is indeed available on st.com.

    This is the X-CUBE-CLASSB-U5, rev4.0.0, delivered as compiler independant certified object code, with the associated UL certificate.

    The package contains project examples with trustzone enabled or trustzone disabled. Please download the package and refer to the readme file and user guide.

    Explorer
    May 29, 2023

    Hello Support team,

    Have a good day.

    we have found the UL/IEC60703 certification for the STM32U5 series below the link

    https://www.st.com/resource/en/certification_document/e480533-20220630-certificateofcompliance.pdf

    But we have some queries which I mentioned below

    1. How to run class B library code in a secure region (can I establish a timer ISR and access the class B lib API in ISR Routine? )Please share examples with us if you have any.

    2. if we do not enable a trust zone so can I use the same MCU as the non-secure region, also can we able to use dual bank and SBSFU functionality(In Disble trust zone configuration)?

    Thanks & Regards

    Hiren R. Thumar