Question
Random Glitches in CSV Output Using SDIO, DMA, and FreeRTOS on STM32F405
I am working on a data logger project using SDIO with DMA and FreeRTOS. The only sensor currently in use is the BME280, which is working fine. However, I am encountering issues when writing the CSV file, such as glitches, character repetition, and other seemingly random problems.





Here is the relevant code:
/* USER CODE BEGIN Header_StartSDTask */
#define BUFFER_SIZE 4096
#define BUFFER_THRESHOLD BUFFER_SIZE/4*3
#define HEADER "Time;BaroTemperature;BaroPressure;BaroHumidity;PitotTemperature;PitotDiffPressure;Latitude;Longitude;IMUax;IMUay;IMUaz;IMUgx;IMUgy;IMUgz;IMUmx;IMUmy;IMUmz\n"
char buffer[BUFFER_SIZE] = HEADER;
uint8_t sensorsResponse;
uint16_t adress = sizeof(HEADER) - 1;
uint32_t maxAdress;
uint32_t lastTime;
uint16_t count = 0;
uint16_t count2 = 0;
char adressCarac;
void bufferize() {
adress += snprintf(&buffer[adress], (BUFFER_SIZE - adress), "%lu;", lastTime);
// Additional sensor data processing...
}
/**
* @brief Function implementing the SDTask thread.
* @PAram argument: Not used
* @retval None
*/
/* USER CODE END Header_StartSDTask */
void StartSDTask(void *argument) {
/* USER CODE BEGIN StartSDTask */
uint8_t sensorID;
uint8_t writeCount;
logger.initialize();
logger.createFile("log.csv");
/* Infinite loop */
for (;;) {
while (osMessageQueueGet(SensorsQueueHandle, &sensorID, NULL, osWaitForever) == osOK) {
// Sensor data processing...
if (adress >= BUFFER_THRESHOLD) {
// Clearing the buffer after the threshold
logger.write(buffer, adress + 1);
writeCount++;
memset(buffer, 0, BUFFER_SIZE);
maxAdress = maxAdress > adress ? maxAdress : adress;
adress = 0;
if (writeCount >= 10) {
logger.flush();
writeCount = 0;
}
}
}
}
/* USER CODE END StartSDTask */
}
- The BME280 sensor is functioning properly.
- The issue arises when writing to the .csv file, with glitches, character repetition, and other random problems.
- I have monitored the task stack, which is using about 500 words of the 9000 available.
- I suspected that the problem could be related to the use of snprintf, but I did not find any issues like .. or .xx. in the buffer.
- I tried increasing the clockdivider to 4, but the problem persists.
- I believe the issue may be related to FreeRTOS preemption, but I have enabled NewLibReentrant and FS_REENTRANT, and no other task uses the SDIO or FATFS.