Read/Write into SD card using FatFs in STM32u5A9
Hello,
I have been trying to read/write into an SD card using the SPI or SDMMC method with Fatfs. I wasn't able to make use of the filex option for file operation which is provided in the STM32u5A9 libraries, since I am using FreeRTOS in my project (as per notes, Filex cannot be used with FreeRTOS). So, I have taken the FatFs library from STM32F4 design and ported the same to STM32U5A9 design (took reference from https://deepbluembedded.com/stm32-sd-card-spi-fatfs-tutorial-examples/). Unfortunately, in both SPI and SDMMC methods, I was not able to initialize my SD card and the application keep on waiting for SPI Rx data in SPI mode, and in SDMMC method, the application keeps on waiting in a HAL_Delay() in HAL_SD_initcard() API

Is there any known issues in this board type? Can you point any working examples for STM32U5A9 with FatFs and FreeRTOS?
Your support is much appreciated!
Thanks & Regards