Skip to main content
Visitor II
March 18, 2024
Solved

Regarding NO STM32 MCU Connected

  • March 18, 2024
  • 2 replies
  • 6252 views

Hello Team,

 

I have connected the STM32H723ZI2 board to the PC, i could see the virtual drive connection to the PC, but when I use the embedded coder support and generate code and try to flash the board it showing No board connection to the board.

 

 

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    The board name would suggest it's a NUCLEO-H743ZI2 with an ST-LINK/V3

    2 replies

    Technical Moderator
    March 18, 2024

    Hello @mvenkat86 ,

    What ST-LINK are you using? Try upgrade the ST-Link firmware.

    Did you try to use latest release of STM32CubeProgrammer?

    Check that the pins are properly connected and make sure that the power supply VDD from the application board is connected to the ST-LINK/V2. (Edit: I mean ST-LINK/V3)

    You can share the schematic for further check.

    This FAQ may help you: Why my STM32 doesn't start? - STMicroelectronics Community.

    Graduate II
    March 18, 2024

    The board name would suggest it's a NUCLEO-H743ZI2 with an ST-LINK/V3

    mvenkat86Author
    Visitor II
    March 19, 2024

    Hello Tesla,

    I checked with STM32cubeprogrammer, the board is connected but it is not detecting with the MATLAB support package in the hardware target connection.

     

    BR

    Venkat

    Visitor II
    March 31, 2024

    Have you solved this problem? I can't connect my H743 board to Simulink. Should I use STLink V3?

    mvenkat86Author
    Visitor II
    March 31, 2024

    I had some setting issues in linking the matlab with stm32 cube mx ide, this is how the problem solved, I am not sure if it is related to the ST link V3