Skip to main content
Graduate
June 6, 2025
Question

Regarding USB Packet Size changes

  • June 6, 2025
  • 1 reply
  • 263 views

Hello there, I'm using USB CDC application. I'm in a situation of receiving more than 250 bytes of data from the Windows(QT). Now my doubt is when the data is more than 64 bytes the USB FS it'll not consider right.
But i revised some websites from there i came to know that "you can send larger than 64 bytes the usb will take care for multiplying the packets". But in my case it was not working. Later from our STM community i came to know that by changing this " CDC_DATA_FS_MAX_PACKET_SIZE" to larger number we can achieve receiving large number of packets.
initially CDC_DATA_FS_MAX_PACKET_SIZE is 64U. Now I've changed to 256U. 

Now it's working fine, but i don't know about later. Does it cause any problems?

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    July 9, 2025

    hello @bsn_14 

    Despite not encountering any issues when replicating your case on my end, I recommend manipulating the internal buffer size for data reception. Most STM32 products support buffer sizes larger than 250 bytes, which allows you to handle bigger data chunks efficiently while letting the USB controller manage packetization according to the USB FS protocol.

    BR

    Gyessine