Skip to main content
Graduate II
November 1, 2025
Question

Require resources of the STM32U599J-DK (ES)

  • November 1, 2025
  • 1 reply
  • 226 views

Hello.

I got a STM32U599J-DK engineering sample from the ST official warehouse (don't ask me how I get this cuz I don't know either).

MB1829-U599 NJQ-B01

A223400084

I searched the st.com and was unable to locate its resources.(user manual, datasheet, data brief, OBD binary).

I wonder if any ST employee got these resources and send them to me if you please as I wish to reuse this board to it's full extent.

Or, are its resources compatible with the STM32U5A9J-DK's? If so, please send me an original OBD demo of the STM32U599J-DK if available.

Thanks in advance.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    November 2, 2025

    Dear @Nathan_Xi ,

    You can use the same package as STM32U5A9J-DK ( Crypto HW difference versus U599 part), However as this is “ES” it may happen this is an early version of either board or Soldered MCU part before full production and Not sure we can provide exact demo if the production one is not running .

    have a great day 

    STOne-32

    Nathan_XiAuthor
    Graduate II
    November 3, 2025

    Thanks.

    I'm glad that the u5a9 package is compatible.

    The demo is like this. It's the very first version.

    Do you have this binary? Please send it to me if available.

    Thanks.

    4977.jpg

    ST Employee
    December 10, 2025

    Hello @Nathan_Xi ,

    to get the Demo OOB, i found the following Item / thread ( about STM32U5G9J-DK1 ) :

    Solved: STM32U5G9J-DK1 Demo Code - STMicroelectronics Community

    and this one : 

    STM32U5G9J- Dk board source code - STMicroelectronics Community

    The OOB demo of the STM32U5G9J-DK1 is not compatible with STM32U5A9J-DK , but STM32U5A9J-DK OOB demo may be available also on TouchGFXDesigner | Software - STMicroelectronics

     

    Best Regards,