Skip to main content
Graduate II
February 11, 2025
Question

RESTful POST requests with LwIP with Nucleo F429ZI

  • February 11, 2025
  • 1 reply
  • 470 views

Hi All,
Dears.

I am studying how to make http requests with Nucleo-F429ZI. I have already had success with the web server example (HTTP Server), but now I need to make requests on another server, where a number of endpoints will be available. The difficulty I am having is that all the examples I found use the GET method, and I need to make some requests with the POST method. Is this possible?

Could you recommend some reading material with examples?

    This topic has been closed for replies.

    1 reply

    ST Employee
    June 23, 2025

    Hi,

    the two following references are not HTTP tutorials, but embedded implementation that may be helpful:

     

    X-CUBE-CLD-GEN STM32Cube Expansion Package contains application examples which connect to cloud platforms over REST requests.It is based on FreeRTOS kernel and LwIP TCP/IP stack.

    The Groovestreams example uses PUT requests.

    The Exosite example uses POST requests.

     

    For new developments, a maintained embedded library such as coreHTTP could be considered.