RMII interface stops working below 3.27V input of STM32H743VIT6
Hi,
I have used STM32H743VIT6 to manage Marvell Ethernet Switch 88E6352
Since last 2 weeks I am trying to resolve below issue.
Everything works fine at the 3.35V input. Just reduction of 100mV creates problems on RMII interface.
This voltage levels are measured & verified with calibrated Fluke Multi-meters as well as on calibrated oscilloscopes. The board is running on Rigol Linear DC Power Supply DC712. Ripple measured on 3.3V line is 60mV.
What further can be diagnose in order to resolve this problem?
Feel free to ask if any query.
Thanks,
Aakash