Solved
ROM constants address defines for ADC calibration values not defined as address of const data
I noticed that the ROM constants for ADC calibration values in the LL headers (*_ll_adc.h) are not defined as addresses of const data.
e.g.
#define VREFINT_CAL_ADDR ((uint16_t*) (0x1FF07A2A))
#define TEMPSENSOR_CAL1_ADDR ((uint16_t*) (0x1FF07A2C))
#define TEMPSENSOR_CAL2_ADDR ((uint16_t*) (0x1FF07A2E))
And it should be:
#define VREFINT_CAL_ADDR ((const uint16_t*) (0x1FF07A2A))
#define TEMPSENSOR_CAL1_ADDR ((const uint16_t*) (0x1FF07A2C))
#define TEMPSENSOR_CAL2_ADDR ((const uint16_t*) (0x1FF07A2E))
Trying to write to it probably results in hardfault errors, but it should raise compile errors too in my opinion.