SM32G071xB Configure option bytes from UART
I have Nucleo-G071RB board when I flash the Option Bytes to load from system memory (Bootloader) via ST-link it works with just reset and I can access the Bootloader,
But when I try to edit the Option Bytes via UART, I need to power off the board and power it on again to access the bootloader. (to implement the new Option Bytes),
So is this a bug, and is there any way to work around the power cycle to implement the Option bytes via UART?
Option Byte configuration:
nBoot0 from checked to unchecked