SMT32L4 CAN bootloader not initializing
I have a STM32L431 that jumps to the bootloader using a software jump to 0x1FFF0000.
I verified that the PB8 and PB9 pins are used on my system and I also have a 8MHz crystal soldered.
I let the bootloader run then I send a 0x79 standard identifier with no data at 125kbps using a python script. I check with a logic analyser on both the Tx and Rx pin. I can see my message is being sent to the MCU, but then I get only NAK or even ERROR (series of dominant bit instead of acknowledge).
I tried bombarding the MCU of message and then starting the bootloader, in this case I get a Tx glitch and only NAK on my message.
THen the bootloader just restarts. It does not restarts if I do not send anything so it must be receiving it somehow it just does like it.