Skip to main content
Visitor II
January 14, 2022
Question

SOLVED!!! BUG IN DOCS!!! ETH Transmit Ring Buffer doesn't wrap around (STM32H745ZI)

  • January 14, 2022
  • 2 replies
  • 5776 views

Issue is that:

ETH->DMACTDRLR, // Channel Tx descriptor ring length register (ETH_DMACTXRLR)

ETH_DMACTDRLR_TDRL

opened a bug:

https://github.com/STMicroelectronics/STM32CubeH7/issues/198

current description:

TDRL[9:0]: Transmit Descriptor Ring Length
This field sets the maximum number of Tx descriptors in the circular descriptor ring. The
maximum number of descriptors is limited to 1K descriptors. It is recommended to put a
minimum ring descriptor length of 4.

!!!!!!!!!!!!!!!!!!!!!!!!

But in reality you should put NUMBER_OF_TX_DESCRIPTORS - 1 (MINUS ONE)

!!!!!!!!!!!!!!!!!!!!!!!!

HELP!

I have ring buffer of length 5.

ETH code is running on M4 core.

5 items transmit without issues.

During 5th item transmission I set tail to be 1st item in ring buffer.

After transmission is over ETH->DMACCATDR register points to element after 5th.

// [0] <- I set this as tail when transmitting 5th element
// [1]
// [2]
// [3]
// [4] <- current 5th item being transmitted AND (DMACCATDR) before transmitting 5th item
// [X]

No matter what I set in tail, 6 packet (which is now 1st in ring buffer) is never transmitted. I tried setting tail element 0, 1, 2, 3 ,4, outside buffer element 5 or 6.

// [0] <- current 6th item being transmitted 
// [1] <- I set this as tail when transmitting 6th element
// [2]
// [3]
// [4] 
// [X] <- (DMACCATDR) before transmitting 6th element

Documentation "RM0399 Reference manual" states:

// The DMA automatically wraps around the base address when the end of ring is reached, as
// shown in Figure 841: DMA descriptor ring.

DMACTDRLR = 5

DMACSR = 0x0000c404 (NIS, AIS, ETI, TBU)

    This topic has been closed for replies.

    2 replies

    Graduate II
    January 16, 2022

    The NUMBER_OF_TX_DESCRIPTORS - 1 information is also confirmed by HAL ETH driver and Alister in these topics:

    https://community.st.com/s/question/0D53W00000EGsnU/how-does-ethernet-rx-descriptor-wrapping-work-on-stm32h7

    https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet

    And again there are also the inconsistent naming issues - this time it's "X" vs "D" letters.

    Reference manual: DMACTXRLR and DMACRXRLR.

    CMSIS header files: DMACTDRLR and DMACTDRLR.

    @Imen DAHMEN​, one more significant misinformation to correct in all related H7 reference manuals.

    Technical Moderator
    January 17, 2022

    Hello @Pavel Krupets​ , @Piranha​ ,

    Thank you for reporting the errors and bringing this to my attention.

    I have passed your feedback internally for fix (Internal ticket number 121000)

    (PS: Ticket number 121000, is an internal tracking number and is not accessible or usable by customers).

    Thanks

    Imen