SPI and IIC bus not being free and locks up. Adding/removing code or changing stack size fixes the problem.
I have seen this with the SPI bus 6 months ago. It just just happened with the IIC bus. I am using Cube 1.12.0 and this maybe related to TKube.1 issue "Potential bug in I2C HAL layer (STM32Cube_FW_F4_V1.25.0) in I2C_MemoryTransmit_TXE_BTF() ?".
I have an array[6][3]. If I initialize the first 5(x3) entries in a routine that is not run the code runs as expected under the debugger. If I initialize all 6 (X3) entries the code hangs in in I2CDevice::MemReceive waiting for the bus to be free the first time I try to read a memory. If I replicate the 6th initialization 5 more times the code runs as expected. If I go back to the non working code and increase the stack from 0x2000 to ox2004 it runs as expected. This was repeatable as I showed it to a colleague. When I was seeing the SPI problem if I cycle power (and the code ran from power up) it functions as expected despite just locking up under the debugger.
Stack analysis says I was using less then half the allocated stack.
I was about to try a software reset of the IIC bus to see if that would free it up, but apparently I changed something another file and everything is working as expected.
I feel like I am missing something, but 30 years of experience is telling me this is a debugger issue and not my code. Anyone seen similar or have any thoughts?
Thanks
Rob