SPI with DMA and TFT Display ST7735
Dear STM32 community
I am trying to setup the ST7735 Display (ST7735) with SPI and DMA for a faster refresh rate. Without DMA everything works fine. When i setting up DMA nothing is displayed on the Display.
My DMA and SPI Settings are:




I want to fill the Screen with black color, for this i use the function fillScreen() from GFX_FUNCTIONS.c. To Transmit the data via DMA i have replaced the old functions in ST7735.c with the DMA Transmit function in ST7735_FillRectangle(), ST7735_WriteCommand() and ST7735_WriteData().

For detail view i have attached the main.c file and the library files from the Display (ST7735.c and GFX_FUNCTIONS.c). I am using a Nucleo-G474RE Boeard with STM32 Version 1.15.1.
I really someone of you guys could help me.
Thanks a lot for your time!
Best regards,
Raphael