Split data from a float array into an uint8_t array
Hi,
I just stumbled upon something interesting (at least for me). For my current project I need to store data from a float array with two elements in an uint8_t array with eight elements. I use the following code to archive this:
pnt = (uint8_t*)out;
for(i = 0; i < 8; i++)
{
uart_tx_buffer[i + 3] = *(pnt + i);
}While it technically works, the bytes from each float element get stored in the buffer in a reversed order. I can give you an example from what I am looking at in the debug session. The float array has the values out = {0x41bef708, 0x4478a1d7}. So the result I exacted for the buffer is uart_tx_buffer = {xx, xx, xx, 0x41, 0xbe, 0xf7, 0x08, 0x44, 0x78, 0xa1, 0xd7}. But in reality it looks like this uart_tx_buffer = {xx, xx, xx, 0x08, 0xf7, 0xbe, 0x41, 0xd7, 0xa1, 0x78, 0x44}.
At first I thought the values in the buffer are completely random because I made a mistake. It took me a while to figure this out. What is the reason why this happens? Can I avoid this, because now I would have to shift all these bytes around.
I am using STM32CubeIDE 1.19.0 to program a NUCLEO-F429ZI.