ST-Link Chipset
Does ST manufacturer a chip that allows integration into a project which provides USB to SWD for the additional ST32 chips? I would like to remove the need for an external programmer and just be able to add a preconfigured USB to SWD SW-Link bridge into a custom program. I guess I am looking for something similar to what ESP32 is now doing. The new EPS32 system has fabric built into the chip which provides direct SWD through the USB interface therefore removing the need for a programming header and external programmer.