ST Link virtual COM Port issue with Excel VBA but shown in other Terminal Software
Hello
I am encountering an issue with a code running on an STM32F4xxx board. The code is designed to perform a measurement, and I aim to transfer this data to a computer. While I can successfully receive the measurement using various terminal programs, I require the data to be imported into an Excel sheet. To facilitate this, I've developed a macro that extracts data from the serial interface.
However, I've encountered a problem where the data from the ST Link Virtual COM port isn't being received by Excel VBA, despite ensuring that all settings such as baud rate, parity, stop bits, and flow control are correctly configured.
Concurrently, I've conducted a test using an Arduino, where I've programmed it to transmit identical data (excluding measurements, which remain constant). Interestingly, when I switch the COM port to that of the Arduino, Excel successfully receives the data.
This leads me to speculate whether there's a discrepancy between the virtual COM port of the STM32F4 Nucleo board and that of an Arduino, particularly in how software addresses the COM port under Windows.
Please note that the PC where the data reception application runs only supports the execution of VBA macros within Excel, and no additional software can be installed.
Thank you for your assistance in resolving this matter.
Best regards,
Lutz