STM32 act as SPI Master and slave for Echo of 1byte Data
MASTER SIDE
uint8_t txByte_master = 0xA5; // Byte to send
uint8_t rxByte_master = 0x00; // Received byte
volatile uint16_t count = 0;
uint8_t dummyTx = 0x00;
uint8_t dummyRx = 0x00;
volatile uint8_t spi_ready = 0; // Flag to indicate SPI transfer complete
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_SPI1_Init(void);
int main(void)
{
HAL_Init();
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_SPI1_Init();
while (1)
{
spi_ready = 0; // Reset flag
// Start SPI communication
HAL_SPI_TransmitReceive_IT(&hspi1, &txByte_master, &rxByte_master, 1);
// Wait until the transaction completes
while (spi_ready == 0);
// Check if received data is correct
if (rxByte_master== 0xA5) {
HAL_SPI_DeInit(&hspi1);// HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_13); // Blink LED if correct
}
HAL_Delay(500); // Delay for visibility
}
/* USER CODE END 3 */
}
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi) {
if (hspi->Instance == SPI1) {
spi_ready = 1; // Set flag to indicate transfer complete
}
}
SLAVE SIDE
uint8_t rxByte_slave = 0x00; // Received byte
uint8_t txByte_slave = 0x00; // Byte to send back (Echo)
uint8_t txByte_slave_check = 0xCE; // Byte to send back for check
volatile uint8_t spi_ready = 0; // Flag to indicate SPI transfer complete
int main(void)
{
HAL_Init();
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_SPI1_Init();
while (1)
{
spi_ready = 0; // Reset flag
HAL_SPI_Receive_IT(&hspi1, &rxByte_slave, 1);
while (spi_ready == 0);
txByte_slave = rxByte_slave;
spi_ready = 0; // Reset flag
HAL_SPI_Transmit_IT(&hspi1, &txByte_slave, 1);
while (spi_ready == 0);
}
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi) {
if (hspi->Instance == SPI1) {
spi_ready = 1; // Set flag indicating reception complete
}
}
void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) {
if (hspi->Instance == SPI1) {
spi_ready = 1; // Set flag indicating transmission complete
}
}
Above written code is for master and slave in which I am trying to echo 1 Byte of Data
through SPI Protocol, here on I am able to capture exact 8 bit of data on slave side but
when slave transmit the same data to master, then master is unable to capture the exact data
and capture some random data.
try to help me in order to solve this problem....
Both side means Master and Slave the board I am using is NUCLEO-F401RE
Note :
I have set the slave side on External oscillator.